Murrelektronik

You are here: Murrelektronik – stay connected / News / Press / Press Releases / Detail page

Press Releases

Apr 15, 2016

Murrelektronik at Hannover Messe 2016

Murrelektronik presents Smart Automation Solutions - April 25 – 29, 2016, Hall 9, Booth D27

The specialist for decentralized automation technology introduces SmartCore technology in their connectors, predictive maintenance for even longer lifetimes and shorter downtimes of power supplies, and IODD On Board, the easy to use configuration tool for IO Link.

The intense network of machines and systems offers many opportunities to improve your customer’s competitive advantage. Murrelektronik offers modern components with innovative features and powerful diagnostic tools. The focus is always on our customers’ needs: easy installation, quick commissioning, less downtime and detailed diagnostics. Concrete examples of this include…

IODD On Board
Murrelektronik revolutionizes IO-Link by providing IODD On Board technology that helps you get your machines and systems up and running faster. IODD On Board programs the IO-Link master from the PLC. Murrelektronik is the first manufacturer to offer this kind of technology, which is the true embodiment of Plug & Play!

SmartCore Technology
The new Murrelektronik cordsets are part of a research project* that developed early detection of a cable that is about to break. This predictive diagnostic function is called SmartCore technology and makes cordsets intelligent. Integrated diagnostics predict when the cordset has reached ca. 80 percent of its lifetime. This feature allows maintenance to change out a cordset before its lifetime expires and it causes expensive downtime.

Predictive Maintenance
In the Emparro product family, the 3-phase, 40A power supply is able to inform maintenance of the perfect time to change out the device. Predictive maintenance enables system service to be planned optimally thereby reducing downtime and any associated costs. This isn’t the only benefit the Emparro family has to offer – with buffer modules, filters and IP67 power supplies for decentralized installations, the product range is ideal for building a first-class power system.

Hannover Messe Press Conference
Murrelektronik will host its press conference about these highlights and much more during the Hannover Messe. Visit us at 9:30am on Wednesday, April 27, 2016 to attend the English press conference and enjoy a cup of coffee from our German Barista Champion!